| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Sub ApplyRectangularPanelArray( _ ByVal panelArray As RectangularAntennaPanelArray _ ) | |
| C# | |
|---|---|
public abstract void ApplyRectangularPanelArray( RectangularAntennaPanelArray panelArray ) | |
| C++/CLI | |
|---|---|
public: abstract void ApplyRectangularPanelArray( RectangularAntennaPanelArray^ panelArray ) | |
Parameters
- panelArray
- the rectangular antenna panel array which is used to generate the antenna position array.
Customer can first define a RectangularAntennaPanelArray, then use this method to set the coordinates of the elements based on the antenna array settings.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00