Keysight 89600 VSA .NET API
ElementDefinition Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > AntennaConfiguration Class : ElementDefinition Property


Glossary Item Box

Gets a reference to the antenna element definition.

Syntax

Visual Basic (Declaration) 
Public MustOverride ReadOnly Property ElementDefinition As AntennaElementDefinition
C# 
public abstract AntennaElementDefinition ElementDefinition {get;}
C++/CLI 
public:
abstract property AntennaElementDefinition^ ElementDefinition {
   AntennaElementDefinition^ get();
}

Remarks

AntennaElementDefinition, it defines the radiation pattern for each antenna element in the antenna array. With the antenna element coordinates set by SetCoordinatesOfElements and the definition for each antenna element, Beam pattern of the signal can be calculated after the beam weights on all antenna elements are demodulated. When this antenna element definition is used, the assumption is all the antenna element have the same radiation pattern.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also