| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Function Remove( _ ByVal item As CarrierMapping _ ) As Boolean | |
| C# | |
|---|---|
public abstract bool Remove( CarrierMapping item ) | |
| C++/CLI | |
|---|---|
public: abstract bool Remove( CarrierMapping^ item ) | |
Parameters
- item
- CarrierMapping to remove from the collection
Return Value
True, if the CarrierMapping was removed from the collection. False otherwise.The maximum number of CarrierMapping items is 32, the minimum is 1.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)