| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Function Remove( _ ByVal item As ComponentCarrier _ ) As Boolean | |
| C# | |
|---|---|
public abstract bool Remove( ComponentCarrier item ) | |
| C++/CLI | |
|---|---|
public: abstract bool Remove( ComponentCarrier^ item ) | |
Parameters
- item
- ComponentCarrier to remove from the collection
Return Value
True, if the ComponentCarrier was removed from the collection. False otherwise.The maximum number of ComponentCarrier items is 32, the minimum is 1.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)