Gets the start CRB and number of CRB of all guard bands for the specified numerology.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Function GetGuardBands( _
ByVal mu As Numerology _
) As Integer() |
Parameters
- mu
- The numerology for which the guard bands to be get.
Return Value
An array of start CRB and number of CRB of all guard bands for the specified numerology.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 25.20
See Also