Keysight 89600 VSA .NET API
IsSearchSpaceModeEnabled Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > ComponentCarrier Class : IsSearchSpaceModeEnabled Property


Glossary Item Box

Gets or sets a value indicating whether PDCCH search space mode is enabled.

Syntax

Visual Basic (Declaration) 
Public Overridable Property IsSearchSpaceModeEnabled As Boolean
C# 
public virtual bool IsSearchSpaceModeEnabled {get; set;}
C++/CLI 
public:
virtual property bool IsSearchSpaceModeEnabled {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true

Remarks

When search space mode is enabled, multiple PDCCH channels can share the same search space. When search space mode is disabled, each PDCCH channel is automatically associated with a search space using zero-base index. PDCCH0 is associated with search space 0, PDCCH1 is associated with search space 1, etc...

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.20

See Also