| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Function Remove( _ ByVal item As Coreset _ ) As Boolean | |
Parameters
- item
- PDCCH to remove from the collection
Return Value
True, if the PDCCH was removed from the collection.| Exception | Description |
|---|---|
| System.InvalidOperationException | when either the item is in used or its index is smaller than one of in used indexes |
Note the first element in the collection cannot be removed because it is the primary PDCCH.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)