Keysight 89600 VSA .NET API
Remove() Method
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > CsirsCollection Class > Remove Method : Remove() Method


Glossary Item Box

Removes the last CSI-RS from the collection.

Syntax

Visual Basic (Declaration) 
Public Overloads Overridable Function Remove() As Boolean
C# 
public virtual bool Remove()
C++/CLI 
public:
virtual bool Remove(); 

Return Value

True, if the CSI-RS was removed from the collection.

Remarks

Note the first element in the collection cannot be removed because it is the primary CSI-RS.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also