| Visual Basic (Declaration) | |
|---|---|
Public Overloads MustOverride Function Remove( _ ByVal item As Csirs _ ) As Boolean | |
Parameters
- item
- CSI-RS to remove from the collection
Return Value
True, if the CSI-RS was removed from the collection.Note the first element in the collection cannot be removed because it is the primary CSI-RS.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)