Keysight 89600 VSA .NET API
CustomModulationFormat Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : CustomModulationFormat Enumeration


Glossary Item Box

Specifies the Custom defined modulation format Condition

Syntax

Visual Basic (Declaration) 
Public Enum CustomModulationFormat 
   Inherits System.Enum
C# 
public enum CustomModulationFormat : System.Enum 
C++/CLI 
public enum class CustomModulationFormat : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
OffCustom modulation format is OFF.—
Psk8the modulation format is 8PSK.—
Qam1024the modulation format is 1024QAM.—
UserDefinedthe modulation format is user defined.27.00
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Remarks

In order to support non-standard compliant modulation format, three modes are defined for custom defined modulation format.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.20

See Also