Keysight 89600 VSA .NET API
DciFormat Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : DciFormat Enumeration


Glossary Item Box

Enum values indicating the DCI format.

Syntax

Visual Basic (Declaration) 
Public Enum DciFormat 
   Inherits System.Enum
C# 
public enum DciFormat : System.Enum 
C++/CLI 
public enum class DciFormat : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Format00DCI Format 0_0—
Format01DCI Format 0_124.20
Format10DCI Format 1_0—
Format11DCI Format 1_124.20
UnsupportedDCI format not supported—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also