Keysight 89600 VSA .NET API
DmrsConfigType Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : DmrsConfigType Enumeration


Glossary Item Box

Enum values indicating the DMRS configuration type

Syntax

Visual Basic (Declaration) 
Public Enum DmrsConfigType 
   Inherits System.Enum
C# 
public enum DmrsConfigType : System.Enum 
C++/CLI 
public enum class DmrsConfigType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Type1DMRS configuration type is Type 1.—
Type2DMRS configuration type is Type 2.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also