Keysight 89600 VSA .NET API
EvmCalculationFrequencyBasis Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : EvmCalculationFrequencyBasis Enumeration


Glossary Item Box

Enum values indicating the EVM calculation Frequency basis.

Syntax

Visual Basic (Declaration) 
Public Enum EvmCalculationFrequencyBasis 
   Inherits System.Enum
C# 
public enum EvmCalculationFrequencyBasis : System.Enum 
C++/CLI 
public enum class EvmCalculationFrequencyBasis : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AllREsEVM calculation is All REs in frequency domain.—
RBEVM calculation is per RB in frequency domain.—
REEVM calculation is per subcarrier in frequency domain.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Remarks

The choice determines the minimum frequency unit for the basic EVM calculation.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also