Keysight 89600 VSA .NET API
EvmCalculationTimeBasis Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : EvmCalculationTimeBasis Enumeration


Glossary Item Box

Enum values indicating the EVM Calculation time basis.

Syntax

Visual Basic (Declaration) 
Public Enum EvmCalculationTimeBasis 
   Inherits System.Enum
C# 
public enum EvmCalculationTimeBasis : System.Enum 
C++/CLI 
public enum class EvmCalculationTimeBasis : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
SlotEvm Calculation basic unit is per slot.—
SubframeEvm Calculation basic unit is per subframe.—
SymbolEvm Calculation basic unit is per symbol.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Remarks

The choice determines which symbols are included for the basis EVM calculation

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also