Keysight 89600 VSA .NET API
Lmax Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : Lmax Enumeration


Glossary Item Box

Enum value indicating the maximum number of possible SS/PBCH blocks in a transmission opportunity.

Syntax

Visual Basic (Declaration) 
Public Enum Lmax 
   Inherits System.Enum
C# 
public enum Lmax : System.Enum 
C++/CLI 
public enum class Lmax : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
L4The maximum number of possible SS/PBCH blocks per transmission opportunity is 4.—
L64The maximum number of possible SS/PBCH blocks per transmission opportunity is 64.—
L8The maximum number of possible SS/PBCH blocks per transmission opportunity is 8.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.00

See Also