Keysight 89600 VSA .NET API
MbsfnRadioFrameAllocationPeriod Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : MbsfnRadioFrameAllocationPeriod Enumeration


Glossary Item Box

Enum value indicating the MBSFN subframe allocation period in frames

Syntax

Visual Basic (Declaration) 
Public Enum MbsfnRadioFrameAllocationPeriod 
   Inherits System.Enum
C# 
public enum MbsfnRadioFrameAllocationPeriod : System.Enum 
C++/CLI 
public enum class MbsfnRadioFrameAllocationPeriod : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
N1The MBSFN subframe allocation period is 1 frame.—
N16The MBSFN subframe allocation period is 16 frames.—
N2The MBSFN subframe allocation period is 2 frames.—
N32The MBSFN subframe allocation period is 32 frames.—
N4The MBSFN subframe allocation period is 4 frames.—
N8The MBSFN subframe allocation period is 8 frames.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also