Keysight 89600 VSA .NET API
ApplyRectangularAntennaArray Method
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > MeasurementExtension Class : ApplyRectangularAntennaArray Method


antennaCenterFrequency
The frequency used to define the element spacing if the elementSpacingUnit is ElementSpacingUnit.WaveLength.
elementSpacingUnit
Indicates the unit of parameter "elementSpacingOnYAxis" and parameter "elementSpacingOnZAxis"/>.
antennaGroupNumber
The antenna group number.
elementNumberOnYAxis
The element number on Y Axis(horizontal) of the Rectangular Antenna Array.
elementNumberOnZAxis
The element number on Z Axis(vertical) of the Rectangular Antenna Array.
elementSpacingOnYAxis
The element spacing on Y Axis(horizontal) of the Rectangular Antenna Array.
elementSpacingOnZAxis
The element spacing on Z Axis(vertical) of the Rectangular Antenna Array.

Glossary Item Box

Applies the Rectangular antenna array parameters to generate the antenna position array.

Syntax

Visual Basic (Declaration) 
Public Overridable Sub ApplyRectangularAntennaArray( _
   ByVal antennaCenterFrequency As Double, _
   ByVal elementSpacingUnit As ElementSpacingUnit, _
   ByVal antennaGroupNumber As Integer, _
   ByVal elementNumberOnYAxis As Integer, _
   ByVal elementNumberOnZAxis As Integer, _
   ByVal elementSpacingOnYAxis As Double, _
   ByVal elementSpacingOnZAxis As Double _
) 
C++/CLI 
public:
virtual void ApplyRectangularAntennaArray( 
   double antennaCenterFrequency,
   ElementSpacingUnit elementSpacingUnit,
   int antennaGroupNumber,
   int elementNumberOnYAxis,
   int elementNumberOnZAxis,
   double elementSpacingOnYAxis,
   double elementSpacingOnZAxis
) 

Parameters

antennaCenterFrequency
The frequency used to define the element spacing if the elementSpacingUnit is ElementSpacingUnit.WaveLength.
elementSpacingUnit
Indicates the unit of parameter "elementSpacingOnYAxis" and parameter "elementSpacingOnZAxis"/>.
antennaGroupNumber
The antenna group number.
elementNumberOnYAxis
The element number on Y Axis(horizontal) of the Rectangular Antenna Array.
elementNumberOnZAxis
The element number on Z Axis(vertical) of the Rectangular Antenna Array.
elementSpacingOnYAxis
The element spacing on Y Axis(horizontal) of the Rectangular Antenna Array.
elementSpacingOnZAxis
The element spacing on Z Axis(vertical) of the Rectangular Antenna Array.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.20

See Also