Keysight 89600 VSA .NET API
ArePrachTimeAdvanceResultsRelativeToTrigger Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > MeasurementExtension Class : ArePrachTimeAdvanceResultsRelativeToTrigger Property


Glossary Item Box

Gets or sets a value indicating whether the PRACH Time Advance results are relative to the trigger for the carriers. See CarrierMapping.ArePrachTimeAdvanceResultsRelativeToTrigger. The getter gets the value from the first carrier and the setter sets the value for all carriers.

Syntax

Visual Basic (Declaration) 
Public Overridable Property ArePrachTimeAdvanceResultsRelativeToTrigger As Boolean
C# 
public virtual bool ArePrachTimeAdvanceResultsRelativeToTrigger {get; set;}
C++/CLI 
public:
virtual property bool ArePrachTimeAdvanceResultsRelativeToTrigger {
   bool get();
   void set (    bool value);
}

Property Value

The default value is false.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 28.40

See Also