Gets or sets a value indicating the power threshold in dB used in detecting the sidelobes to be included in the beam pattern summary.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property BeamPatternSidelobeDetectionThreshold As Double |
| C# | |
|---|
public virtual double BeamPatternSidelobeDetectionThreshold {get; set;} |
| C++/CLI | |
|---|
public:
virtual property double BeamPatternSidelobeDetectionThreshold {
double get();
void set ( double value);
} |
Property Value
The default value is -20.0.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 29.40
See Also