Keysight 89600 VSA .NET API
BeamWeightsFormat Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > MeasurementExtension Class : BeamWeightsFormat Property


Glossary Item Box

Gets or sets a value indicating display format for beam weights results.

Syntax

Visual Basic (Declaration) 
Public Overridable Property BeamWeightsFormat As BeamWeightsFormat
C# 
public virtual BeamWeightsFormat BeamWeightsFormat {get; set;}
C++/CLI 
public:
virtual property BeamWeightsFormat BeamWeightsFormat {
   BeamWeightsFormat get();
   void set (    BeamWeightsFormat value);
}

Property Value

The default value is BeamWeightsFormat.Cartesian.

Remarks

Beam weight values are complex (I+jQ) values. The display format is as follows. Note displayed angles are in units of degrees.
Agilent.SA.Vsa.NewRadio.BeamWeightsFormat.#ctor Display of 1 - j1
BeamWeightsFormat.Cartesian 1 - j1
BeamWeightsFormat.Polar 1.41 ∠ 315.00
BeamWeightsFormat.LogPolar 3.01 ∠ 315.00

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also