Keysight 89600 VSA .NET API
CopyAutoToManual Method
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > MeasurementExtension Class : CopyAutoToManual Method


Glossary Item Box

Applies auto-detected signal parameters to signal configuration

Syntax

Visual Basic (Declaration) 
Public Overridable Sub CopyAutoToManual() 
C# 
public virtual void CopyAutoToManual()
C++/CLI 
public:
virtual void CopyAutoToManual(); 

Remarks

Currently, only SS block auto detection is able to detect some signal parameters

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also