Keysight 89600 VSA .NET API
EvmWindowLengthMode Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > MeasurementExtension Class : EvmWindowLengthMode Property


Glossary Item Box

Gets or sets the EVM Window Length mode as being 3GPP standard-defined or custom-defined

Syntax

Visual Basic (Declaration) 
Public Overridable Property EvmWindowLengthMode As EvmWindowLengthModeType
C# 
public virtual EvmWindowLengthModeType EvmWindowLengthMode {get; set;}
C++/CLI 
public:
virtual property EvmWindowLengthModeType EvmWindowLengthMode {
   EvmWindowLengthModeType get();
   void set (    EvmWindowLengthModeType value);
}

Property Value

The default value is EvmWindowLengthModeType.Mode3Gpp

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also