| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property EvmWindowLengthSample As Integer | |
| C# | |
|---|---|
public virtual int EvmWindowLengthSample {get; set;} | |
Property Value
The default value is 32 samples. The minimum is 1 sample and the maximum depends on AnalysisBandwidth and SynchronizationType.The value of this property is ignored if EvmWindowLengthMode is set to EvmWindowLengthModeType.Mode3Gpp.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00