Keysight 89600 VSA .NET API
ExtendedFrequencyLockRange Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > MeasurementExtension Class : ExtendedFrequencyLockRange Property


Glossary Item Box

Gets or sets a value indicating the extended frequency lock range.

Syntax

Visual Basic (Declaration) 
Public Overridable Property ExtendedFrequencyLockRange As Double
C# 
public virtual double ExtendedFrequencyLockRange {get; set;}
C++/CLI 
public:
virtual property double ExtendedFrequencyLockRange {
   double get();
   void set (    double value);
}

Property Value

The default value is 0.0 Hz.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 27.00

See Also