Keysight 89600 VSA .NET API
IsEvmConformanceCompliant Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > MeasurementExtension Class : IsEvmConformanceCompliant Property


Glossary Item Box

Gets or sets a value indicating whether the EVM calculation complies with conformance standard.

Syntax

Visual Basic (Declaration) 
Public Overridable Property IsEvmConformanceCompliant As Boolean
C# 
public virtual bool IsEvmConformanceCompliant {get; set;}
C++/CLI 
public:
virtual property bool IsEvmConformanceCompliant {
   bool get();
   void set (    bool value);
}

Property Value

The default value is true.

Remarks

If true, all the equalization/tracking/EVM basic unit setting follow the standard 38.104/38.141 for Downlink and 38.521 for Uplink.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also