Keysight 89600 VSA .NET API
IsSsbBwpMeasurementIndependent Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > MeasurementExtension Class : IsSsbBwpMeasurementIndependent Property


Glossary Item Box

Gets or sets a value indicating whether BWPs and SSBs measurements are independent.

Syntax

Visual Basic (Declaration) 
Public Overridable Property IsSsbBwpMeasurementIndependent As Boolean
C# 
public virtual bool IsSsbBwpMeasurementIndependent {get; set;}
C++/CLI 
public:
virtual property bool IsSsbBwpMeasurementIndependent {
   bool get();
   void set (    bool value);
}

Property Value

The default value is false.

Remarks

If true, the timing/frequency/clock error estimations and compensation are independent for all SSBs and BWPs. If false, the timing/frequency/clock error estimations and compensations are accumulated between all SSBs and BWPs. this feature is to help isolate the configuration issues between SSBs and BWPs

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also