| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property IsTrackAmplitude As Boolean | |
| C# | |
|---|---|
public abstract bool IsTrackAmplitude {get; set;} | |
Property Value
The default value is true.If true, the average amplitude of the subcarriers is tracked. This means that the average amplitude variation of the subcarriers is backed out of all subcarriers before they are used. If there is amplitude droop in the signal, this will cause the droop to be removed and ignored by the measurement. However, if there is no amplitude droop, this could make the measurement slightly less accurate because the tracking may try to compensate amplitude variation that is due to noise.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)