Keysight 89600 VSA .NET API
PdcchBeamPatternEnabled Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > MeasurementExtension Class : PdcchBeamPatternEnabled Property


Glossary Item Box

Gets or sets a value indicating whether PDCCH beam pattern is calculated and displayed in the beam pattern trace.

Syntax

Visual Basic (Declaration) 
Public Overridable Property PdcchBeamPatternEnabled As Boolean
C# 
public virtual bool PdcchBeamPatternEnabled {get; set;}
C++/CLI 
public:
virtual property bool PdcchBeamPatternEnabled {
   bool get();
   void set (    bool value);
}

Property Value

The default value is false.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.00

See Also