| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property PucchDecodeMode As DecodeModeSelection | |
| C# | |
|---|---|
public virtual DecodeModeSelection PucchDecodeMode {get; set;} | |
| C++/CLI | |
|---|---|
public: virtual property DecodeModeSelection PucchDecodeMode { DecodeModeSelection get(); void set ( DecodeModeSelection value); } | |
Property Value
The default value is DecodeModeSelection.NoBitsThe choice determines the bit processing step from which the output bits are displayed in the Decoded Symbol trace. Select DecodeModeSelection.NoBits for best measurement speed.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20