| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property ResultLength As Integer | |
| C# | |
|---|---|
public abstract int ResultLength {get; set;} | |
Property Value
The default value is 10 subframes. The minimum value is 0 subframes and the maximum is 500 subframes.Result Length, along with ResultLengthAdditionalSlots and AnalysisStartBoundary determines the amount of data acquired.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)