| Visual Basic (Declaration) | |
|---|---|
Public MustOverride ReadOnly Property SystemSampleFrequency As Double | |
| C# | |
|---|---|
public abstract double SystemSampleFrequency {get;} | |
Property Value
The default value is 153.6 MHz. The maximum and minimum values are limited by the capabilities of the measurement input hardware.The OFDM subcarrier spacing is equal to SystemSampleFrequency / FftLength.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)