Keysight 89600 VSA .NET API
MimoResultsReferenceSignalType Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : MimoResultsReferenceSignalType Enumeration


Glossary Item Box

Enum values indicating the reference signal type used for MIMO results calculation

Syntax

Visual Basic (Declaration) 
Public Enum MimoResultsReferenceSignalType 
   Inherits System.Enum
C# 
public enum MimoResultsReferenceSignalType : System.Enum 
C++/CLI 
public enum class MimoResultsReferenceSignalType : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
AutoSpecifies the reference signal type used for MIMO results is auto detected, which is the signal which has max power on one of the channel.—
CsirsSpecifies the reference signal type used for MIMO results is CSI-RS.—
IndividualSpecifies the reference signal type used for MIMO results is the reference signal of each individual channel.—
PdcchDmrsSpecifies the reference signal type used for MIMO results is PDCCH DMRS.—
PdschDmrsSpecifies the reference signal type used for MIMO results is PDSCH DMRS.—
PuschDmrsSpecifies the reference signal type used for MIMO results is PUSCH DMRS.—
SrsSpecifies the reference signal type used for MIMO results is SRS.—
SsbSpecifies the reference signal type used for MIMO results is SSB.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.00

See Also