Keysight 89600 VSA .NET API
ModulationFormat Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : ModulationFormat Enumeration


Glossary Item Box

Enum values indicating modulation format.

Syntax

Visual Basic (Declaration) 
Public Enum ModulationFormat 
   Inherits System.Enum
C# 
public enum ModulationFormat : System.Enum 
C++/CLI 
public enum class ModulationFormat : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
BpskModulation format is BPSK—
Bpsk45DegreeBPSK with 45 Degree rotation—
BpskHalfPIModulation format is BPSK-PI/2 (square)23.20
NoneModulation format is not specified—
Qam1024Modulation format is 1024-QAM (square)26.20
Qam16Modulation format is 16-QAM (square)—
Qam256Modulation format is 256-QAM (square)—
Qam64Modulation format is 64-QAM (square)—
QpskModulation format is QPSK—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also