Keysight 89600 VSA .NET API
MultichannelAnalysisMode Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : MultichannelAnalysisMode Enumeration


Glossary Item Box

Enum values indicating the multiple channel analysis mode for the measurement.

Syntax

Visual Basic (Declaration) 
Public Enum MultichannelAnalysisMode 
   Inherits System.Enum
C# 
public enum MultichannelAnalysisMode : System.Enum 
C++/CLI 
public enum class MultichannelAnalysisMode : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
IndividualMultiple channels are analyzed individually.—
MimoMultiple channels are analyzed together as MIMO input channels.—
MimoAndIndividualMultiple channels are analyzed together as MIMO input channels first, then each channel is measured individually.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.00

See Also