Keysight 89600 VSA .NET API
NumberOfSrsSymbols Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : NumberOfSrsSymbols Enumeration


Glossary Item Box

Enum values indicating the number of SRS symbols

Syntax

Visual Basic (Declaration) 
Public Enum NumberOfSrsSymbols 
   Inherits System.Enum
C# 
public enum NumberOfSrsSymbols : System.Enum 
C++/CLI 
public enum class NumberOfSrsSymbols : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
EightSpecifies SRS symbol number as 8 symbol (N8).26.00
FourSpecifies SRS symbol number as 4 symbol (N4).—
OneSpecifies SRS symbol number as 1 symbol (N1).—
TwelveSpecifies SRS symbol number as 12 symbol (N12).26.00
TwoSpecifies SRS symbol number as 2 symbol (N2).—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 25.00

See Also