| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Function Remove( _ ByVal item As Pdcch _ ) As Boolean | |
Parameters
- item
- PDCCH to remove from the collection
Return Value
True, if the PDCCH was removed from the collection.Note the first element in the collection cannot be removed because it is the primary PDCCH.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)