Keysight 89600 VSA .NET API
PdschAutoDetectionMode Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : PdschAutoDetectionMode Enumeration


Glossary Item Box

Enum values indicating the auto-detection mode for PDSCH channels

Syntax

Visual Basic (Declaration) 
Public Enum PdschAutoDetectionMode 
   Inherits System.Enum
C# 
public enum PdschAutoDetectionMode : System.Enum 
C++/CLI 
public enum class PdschAutoDetectionMode : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
OffAuto-detection is disabled.—
PowerBasedAuto-detection is enabled. Power, modulation and RS sequence are auto-detected—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also