Keysight 89600 VSA .NET API
Remove Method
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > PdschCollection Class : Remove Method


item
PDSCH to remove from the collection

Glossary Item Box

Removes the indicated PDSCH from the collection.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function Remove( _
   ByVal item As Pdsch _
) As Boolean
C# 
public abstract bool Remove( 
   Pdsch item
)
C++/CLI 
public:
abstract bool Remove( 
   Pdsch^ item
) 

Parameters

item
PDSCH to remove from the collection

Return Value

True, if the PDSCH was removed from the collection.

Remarks

Note the first element in the collection cannot be removed because it is the primary PDSCH.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also