Gets or sets a value indicating the first symbol index in a slot used by this physical channel.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property FirstSymbolIndex As Integer |
| C# | |
|---|
public abstract int FirstSymbolIndex {get; set;} |
| C++/CLI | |
|---|
public:
abstract property int FirstSymbolIndex {
int get();
void set ( int value);
} |
Property Value
Default value is 0. Range of value is 0 through 13.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also