| Visual Basic (Declaration) | |
|---|---|
Public Overridable ReadOnly Property Nid As Integer | |
| C# | |
|---|---|
public virtual int Nid {get;} | |
Property Value
Default value is ComponentCarrier.CellIdentity. If the NidSource is NidSource.FromCellId, the range from 0 to 1007. Otherwise, the range of value is 0 through 65535.Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.20