Keysight 89600 VSA .NET API
Nscid Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pdsch Class : Nscid Property


Glossary Item Box

Gets or sets a value indicating the SCID value used for DMRS sequence generation.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property Nscid As Integer
C# 
public abstract int Nscid {get; set;}
C++/CLI 
public:
abstract property int Nscid {
   int get();
   void set (    int value);
}

Remarks

Default value is 0. Range of value is 0 or 1.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also