Keysight 89600 VSA .NET API
PtrsL Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pdsch Class : PtrsL Property


Glossary Item Box

Gets or sets a value indicating the start PTRS symbol in time domain.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property PtrsL As PtrsL
C# 
public abstract PtrsL PtrsL {get; set;}
C++/CLI 
public:
abstract property PtrsL PtrsL {
   PtrsL get();
   void set (    PtrsL value);
}

Property Value

Default value is PtrsL.L1.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also