Gets or sets the coreset ID the PDSCH will rate match around/>.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Property RateMatchAroundCoresetId As Integer |
| C# | |
|---|
public virtual int RateMatchAroundCoresetId {get; set;} |
| C++/CLI | |
|---|
public:
virtual property int RateMatchAroundCoresetId {
int get();
void set ( int value);
} |
Property Value
Default value is -1, means no coreset rate match around.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 24.00
See Also