Keysight 89600 VSA .NET API
ReservedCdmGroupNumber Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pdsch Class : ReservedCdmGroupNumber Property


Glossary Item Box

Gets or sets a value indicating the number of DMRS CDM groups without data.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property ReservedCdmGroupNumber As ReservedDmrsCdmGroupNumber
C# 
public abstract ReservedDmrsCdmGroupNumber ReservedCdmGroupNumber {get; set;}
C++/CLI 
public:
abstract property ReservedDmrsCdmGroupNumber ReservedCdmGroupNumber {
   ReservedDmrsCdmGroupNumber get();
   void set (    ReservedDmrsCdmGroupNumber value);
}

Property Value

Default value is ReservedDmrsCdmGroupNumber.One.

Remarks

customer can set this value directly or if customer enables UseAntennaPortsIndex, customer can set AntennaPortsIndex, VSA will derive ReservedCdmGroupNumber from AntennaPortsIndex

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also