| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property TransportBlockTwoMcs As Integer | |
| C# | |
|---|---|
public virtual int TransportBlockTwoMcs {get; set;} | |
Property Value
Default value is 0. Range of value is 0 through 27 or 28, depending on current value of McsTable.The MCS value, along with the McsTable determines the modulation format and coding rate applied to a physical channel transmission.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.20