Keysight 89600 VSA .NET API
TransportBlockTwoRVIndex Property
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace > Pdsch Class : TransportBlockTwoRVIndex Property


Glossary Item Box

Gets or sets a value indicating the transport-block-two RV index.

Syntax

Visual Basic (Declaration) 
Public Overridable Property TransportBlockTwoRVIndex As Integer
C# 
public virtual int TransportBlockTwoRVIndex {get; set;}
C++/CLI 
public:
virtual property int TransportBlockTwoRVIndex {
   int get();
   void set (    int value);
}

Property Value

The default value is 0.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 26.20

See Also