Keysight 89600 VSA .NET API
Periodicity Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : Periodicity Enumeration


Glossary Item Box

Enum values indicating the periodicity for SS/PBCH transmissions

Syntax

Visual Basic (Declaration) 
Public Enum Periodicity 
   Inherits System.Enum
C# 
public enum Periodicity : System.Enum 
C++/CLI 
public enum class Periodicity : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Period10Milliseconds10 milliseconds (one frame)—
Period160Milliseconds160 milliseconds (sixteen frames)—
Period20Milliseconds20 milliseconds (two frames)—
Period40Milliseconds40 milliseconds (four frames)—
Period5Milliseconds5 milliseconds (half-frame)—
Period80Milliseconds80 milliseconds (eight frames)—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 23.00

See Also