Keysight 89600 VSA .NET API
PrachFdm Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : PrachFdm Enumeration


Glossary Item Box

Enum values indicating the number of PRACH occasions in frequency domain in one time stamp

Syntax

Visual Basic (Declaration) 
Public Enum PrachFdm 
   Inherits System.Enum
C# 
public enum PrachFdm : System.Enum 
C++/CLI 
public enum class PrachFdm : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Fdm1The number of PRACH occasions is 1—
Fdm2The number of PRACH occasions is 2—
Fdm4The number of PRACH occasions is 4—
Fdm8The number of PRACH occasions is 8—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also