Keysight 89600 VSA .NET API
PrachFormat Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : PrachFormat Enumeration


Glossary Item Box

Enum values indicating PRACH preamble format

Syntax

Visual Basic (Declaration) 
Public Enum PrachFormat 
   Inherits System.Enum
C# 
public enum PrachFormat : System.Enum 
C++/CLI 
public enum class PrachFormat : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
Format0Preamble format is Format 0—
Format1Preamble format is Format 1—
Format2Preamble format is Format 2—
Format3Preamble format is Format 3—
FormatA1Preamble format is Format A1—
FormatA1B1Preamble format is Format A1/B1—
FormatA2Preamble format is Format A2—
FormatA2B2Preamble format is Format A2/B2—
FormatA3Preamble format is Format A3—
FormatA3B3Preamble format is Format A3/B3—
FormatB1Preamble format is Format B1—
FormatB2Preamble format is Format B2—
FormatB3Preamble format is Format B3—
FormatB4Preamble format is Format B4—
FormatC0Preamble format is Format C0—
FormatC2Preamble format is Format C2—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also