Keysight 89600 VSA .NET API
PrachSubcarrierSpacing Enumeration
See Also 
Agilent.SA.Vsa.NewRadio.Interfaces Assembly > Agilent.SA.Vsa.NewRadio Namespace : PrachSubcarrierSpacing Enumeration


Glossary Item Box

Enum values indicating PRACH subcarrier spacing

Syntax

Visual Basic (Declaration) 
Public Enum PrachSubcarrierSpacing 
   Inherits System.Enum
C# 
public enum PrachSubcarrierSpacing : System.Enum 
C++/CLI 
public enum class PrachSubcarrierSpacing : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
FifteenSubcarrier spacing is 15 kHz—
FiveSubcarrier spacing is 5 kHz—
FourEightySubcarrier spacing is 480 kHz27.40
NineSixtySubcarrier spacing is 960 kHz27.40
OnePointTwentyFiveSubcarrier spacing is 1.25 kHz—
OneTwentySubcarrier spacing is 120 kHz—
SixtySubcarrier spacing is 60 kHz—
ThirtySubcarrier spacing is 30 kHz—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 24.00

See Also